FB#.STOREMULTITURN.BITS
Description
The number of most significant single-turn bits (power of 2 counts) used to determine if the position stored is valid after power cycle and ensures the motor did not move while the power was off.
Context
For more information on how to set FB#.STOREMULTITURN.BITS, see Store Multiturn.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-08-03-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
2-8 |
|
Default Value |
2 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
FB1.STOREMULTITURN.BITS |
3500h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB2.STOREMULTITURN.BITS |
3501h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB3.STOREMULTITURN.BITS |
3502h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB4.STOREMULTITURN.BITS |
3503h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
FB5.STOREMULTITURN.BITS |
3504h |
0eh |
Unsigned8 |
- |
- |
Read/Write |
No |
|
Name |
ID |
Hex |
Data Type |
Access |
Units |
|---|---|---|---|---|---|
|
FB1.STOREMULTITURN.BITS |
30480 |
7710 |
Unsigned8 |
Read/Write |
- |
|
FB2.STOREMULTITURN.BITS |
30481 |
7711 |
Unsigned8 |
Read/Write |
- |
|
FB3.STOREMULTITURN.BITS |
30482 |
7712 |
Unsigned8 |
Read/Write |
- |
|
FB4.STOREMULTITURN.BITS |
30483 |
7713 |
Unsigned8 |
Read/Write |
- |
|
FB5.STOREMULTITURN.BITS |
30484 |
7714 |
Unsigned8 |
Read/Write |
- |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
FB1.STOREMULTITURN.BITS |
30480 |
Unsigned8 |
Read/Write |
- |
|
FB2.STOREMULTITURN.BITS |
30481 |
Unsigned8 |
Read/Write |
- |
|
FB3.STOREMULTITURN.BITS |
30482 |
Unsigned8 |
Read/Write |
- |
|
FB4.STOREMULTITURN.BITS |
30483 |
Unsigned8 |
Read/Write |
- |
|
FB5.STOREMULTITURN.BITS |
30484 |
Unsigned8 |
Read/Write |
- |